| Maintenance knowledge: Bearing mounting - Mechanical bearing mounting |
|||||||||||
|
Mechanical mounting is generally suitable for small bearings. Mounting force can be applied to the bearing by placing a fitting tool impact ring and sleeve against the inner ring and using a press or hammer to advance the bearing to its proper location on the shaft. Be sure the correct size impact ring and sleeve are selected from a bearing fitting tool kit, such as the SKF TMFT 33 fitting tool kit. The bearing should be exactly at right angles to the shaft before beginning, and the shaft lightly lubricated. |
|||||||||||
| Do not apply a sleeve to the outer raceway when mounting on a shaft, or to the inner raceway when mounting in a housing- and NEVER mount by striking the bearing directly with a hammer. | |||||||||||
| Raceway damage incurred when a bearing is incorrectly mounted can result in premature bearing failure. Typical problems, which can cause premature failure, are: | |||||||||||
|
|||||||||||
| Cylindrical shafts - interference fits | |||||||||||
|
Most bearings are fitted to their shaft or housing with one component having an interference fit or in some cases both. For determining the correct fit, refer to the SKF General Catalogue, the SKF Maintenance Handbook or consult an SKF application engineer. |
|||||||||||
| Incorrect mounting | |||||||||||
| When bearings are mounted cold, care must be taken to ensure that the drive-up forces are applied to the ring with the interference fit. Damage and a resulting bearing failure can occur if the mounting force is transmitted through the rolling elements causing damage to the raceways. | |||||||||||
| Correct mounting | |||||||||||
|
The correct way to minimise raceway damage is to use the specifically designed tools from SKF - the TMFT fitting tools series. These tools ensure that the drive-up forces are applied effectively and evenly to the ring with the interference fit avoiding raceway damage. |
|||||||||||
|
|||||||||||
|
Tapered shafts - interference fits |
|||||||||||
|
Bearings mounted on tapered seatings, adapter sleeve or withdrawal sleeve achieve their interference fit by being driven up the tapered shaft. Care should be taken to ensure that the bearing is not driven up too far as all the internal clearance may be removed, which can result in bearing damage. |
|||||||||||
| Spherical roller bearings | |||||||||||
| Method: Correct adjustment of spherical roller bearings is determined by measuring the residual internal clearance in the bearing or by the amount of axial drive-up. | |||||||||||
|
|||||||||||
|
Self-aligning ball bearings |
|||||||||||
| Method: Adjustment of double row, self-aligning ball bearings to obtain a correct interference fit is more difficult to achieve than spherical roller bearings because the feeler gauge method cannot be used. The most effective method to adjust this type of bearing correctly is to use the SKF TMHN 7 lock not spanner set. | |||||||||||
|
|||||||||||
| For more information on SKF fitting tools, please see our Mechanical Tools FAQ section or our online catalogue on this site | |||||||||||